Beli belt tension meter di monotaro.id
Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
- FACOM Belt Tension Meteratribut:
- Engine: Diesel/Petrol
- Material: Plastic
- Timing Pulleys Belt Product Type: Belt Tension Testing
- BANDO Belt Tension Meter (Alat Ukur Ketegangan Belt)Deskripsi:Using the tension meter makes it easy to adjust the tension of the V-belt._x000D_In addition, deflection and load can be measured at the same time.
- Gates Unitta Asia Sonic Belt Tension MeterDeskripsi:Improved measurement sensitivity.Shorter measurement time.Adopts an organic EL display.Full manual installation function.Accessories : Flexible arm microphone (model number: TM-AMM), carrying case, alkaline batteries (2 AAA batteries) *USB cable is not included.atribut:
- Power Supply: Alkaline batteries (AAA x 2)
- Measurement Range (Hz): 10 to 5000
- External Dimensions (mm): 59×160×26
- TESTO Moisture Meter (Alat Ukur Kelembaban)Deskripsi:The testo 616 professional moisture meter provides you with a precise and non-destructive means of measuring the moisture content of wood and building materials and of monitoring the drying process after water damage. Simply select the characteristic curve and place the meter’s measuring claw against the surface of the material you would like to measure. The meter shows you the moisture content as a weight percentage compared to the dry weight. Press the relevant key to save the reading to your meter.Although the measuring claw only comes into contact with the surface, wall or flooring that is being measured, it is able to determine the moisture content of the wood or other material down to a depth of 5 cm.Ideal areas of use for the testo 616 moisture meterThe testo 616 moisture meter is a professional measuring device that can be used in areas as diverse as water damage restoration or carpentry or joinery.Moisture damage detection: the non-destructive method for finding moisture in walls and floorsMonitoring drying processes: from carrying out moisture inspections to meeting building schedules to controlled drying after water damage - the non-destructive method for determining the moisture content in wood and building materialsMoisture in wood: for checking the moisture content of wood that has been stored prior to processingtesto 616 moisture meter with 10 characteristic curvesSoft woodHard woodPressboardAnhydrite screedCement screedLime sand brickGas concreteConcreteHigh insulation bricksBrickwork Product Includes: testo 616 moisture meter for wood and building materials, calibration protocol, batteries.Determining moisture in wood Moisture content is a decisive factor in the further processing and use of timber products. If wood is installed with the wrong moisture content this may result in mechanical deformations (contracting and swelling) at the site where the material is subsequently used, and therefore damage to pieces of furniture or entire supporting structures in buildings. Therefore, before being made into furniture or supporting material by a joiner/carpenter, the suitability of the wood has to be assessed by measuring the moisture content. The testo 616 enables the quick and non-destructive examination of the material moisture characteristics in timber. Characteristic curves are available for measuring wood moisture in soft and hard woods, and chipboard. These characteristic curves were developed in cooperation with the LPI institute.The measurement results are calculated up to a depth of 5 cm and can be recorded at the touch of a button. The readings are displayed in percent by weight in comparison to the dry mass of the material. Monitoring drying processes Whether freshly laid screed, or monitored drying of moisture damage, timely determination of the required moisture level will save time and therefore money. Screeds are laid in the in interior works stage, generally after plastering. The flooring and painting and decorating then follow. The drying behaviour is therefore a significant factor in the works schedule, primarily because the laying of flooring depends on this.The moisture measurement establishes readiness for flooring; liability for the flooring is thus transferred to the respective trade installing the flooring. An important part of this work is therefore documentation and assurance in the testing for readiness for flooring. What is the extent of moisture damage? This question has to be answered in order to decide which instruments are to be used to speed up the drying process.The testo 616 can be used to quickly and non-destructively examine the material moisture in building materials. It also makes work easier when drying processes for floors, walls and surfaces have to be observed. Diagnosing building moisture Moisture may penetrate walls, floors and ceilings due to pipes bursting or water ingress. Some of this moisture damage may not be detected immediately. Rising or ingressing water, faulty rain and waste water drains, or even blocked drains and inadequate seepage capacity may be the cause. Depending on where it is getting out or in, the moisture can spread in different ways; enormous damage may be done if discovered too late. Therefore, measurement of the material moisture in the affected places is necessary to be able to identify the source of the damage. The testo 616 can be used to quickly and non-destructively examine the material moisture in building materials. The measuring clamp is laid on the surface; the value can be read immediately. The measurement results are calculated up to a depth of 5 cm and can be recorded at the touch of a button. The readings are displayed in percent by weight in comparison to the dry mass of the material. For easy, quick handling, characteristics are already stored in testo 616 for the following construction materials: anhydrite screed, cement screed, lime sand brick, aerated concrete, concrete, vertically perforated brick and solid brick; these aid detection of wet places in the construction materials.
- OTC Belt Tension Gaugeatribut:
- UNSPSC: 26111805
- AISIN Oil PumpDeskripsi:AISIN is the No. 1 supplier of oil pumps in the world. All AISIN Oil Pumps are engineered in conjunction with automobile makers during the initial stages of new model vehicle development, years before they enter the market. Using the exact process of development and utilizing the same OE manufacturing plants for production, AISIN Aftermarket Oil Pumps exhibit the same quality, durability, performance, and reliability to that of the OE product.
- RION Pocket Size Vibration MeterDeskripsi:Pocket-size vibration meter with integrated accelerometer, Designed for quick and easy use in the field. Suitable for preventive maintenance of industrial equipment, on-site quality control, product development, etc.atribut:
- Dimensions (mm): 178x64x27
- Applicable Standards: Chinese RoHS, CE marking
- Type: Piezoelectric accelerometer (shear type)
- Measurement Range: Acceleration 0.1 to 199.9 m/s2 EQ PEAK (RMS x √2) Velocity 0.1 to 199.9 mm/s RMS Displacement 0.001 to 1.999 mm EQ P-P (RMS x 2√2)
- Measurement Accuracy (80 Hz): Between -10 ºC and +50 ºC, Outside of temperature range at left
- Vibration Frequency Range: Acceleration 10 Hz to 1 kHz (LO) 1 kHz to 15 kHz (HI). Velocity 10 Hz to 1 kHz. Displacement 10 Hz to 1 kHz
- Load Impedance (kΩ): Approx. 10 or higher
- AC Output (V): Approx. ±2 PEAK
- Power Supply: IEC R6 (size AA) batteries (alkaline / manganese or nickel-hydride rechargeable batteries) x 2
- Current Consumption (mA): Approx. 35
- Battery Life: About 50 h continuous use (at 25 ºC, with alkaline batteries)
- Dimensions (HxWxD) (mm): 178x64x27
- Supplied Accessories: IEC R6 (size AA) alkaline batteries x 2, silicone rubber case x 1,Attachment S x 1
- Output Impedance (ohm): Approx. 170
- Mitsuboshi Belting Non-contact sonic belt tension meter Doctor Tension Type-IV DRT-SH-F1Deskripsi:[A wide variety of belts that can be measured] It can be used with a variety of belts, including timing belts, flat belts, V-belts, and V-ribbed belts. [Belt vibration frequency and tension meter can be displayed simultaneously] [kgf] and [N] can be displayed using the unit switch. [Two types of unit display can be selected] A wide range of frequency ranges from 10.0 to 999 [Hz] (top three digits) can be measured. [Short measurement time due to unique high-speed data processing] Adopting a high-performance one-chip microcomputer and unique data processing allows tension measurement in a short time. (As short as 0.5 seconds) [Equipped with memory function] 10 types of belt condition data and 89 types of unit room data can be stored. [Equipped with auto power off function] The power is automatically turned off 5 minutes after the last operation. This prevents battery consumption due to forgetting to turn off the power switch. [Japanese / English switching possible] When the power is on, you can switch the display between Japanese and English by pressing and holding the "0" and "Enter" keys simultaneously.*This product is the flexible arm sensor head (microphone sensor) only. *The part number for the set including the main unit is DRT-4.atribut:
- Product Name: Flexible arm sensor head
- ROHS Directive (Corresponding to 10 Substances): Correspondence
- Wipro Belt Tension Meter (Alat Ukur Ketegangan Belt)Deskripsi:- Menyesuaikan ketegangan sabuk drive pada berbagai serpentin dan camshaft sabuk ketebalan.- Adjustable dual skala wisuda (Nm) dapat dibaca dari depandan belakang alat.atribut:
- Range (mm): 0-20
- Landtek Vibration MeterDeskripsi:Vibration Meter Landtek digunakan untuk mengukur gerak periodik, untuk memeriksa ketidakseimbangan dan membelokkan bergerak mesin. Specifically dirancang untuk hadir mengukur berbagai getaran mekanis. sehingga untuk provde data untuk kontrol kualitas, waktu dan peralatan pemeliharaan dijalankan. Iuse kinerja tinggi percepatan meter, menyadari repetitiveness dan pengukuran akurat. Ini memiliki fungsi pengujian bantalan poros situasi.
- KRISBOW Tang Pengupas Kabelatribut:
- Size (inch): 6
- Material: Steel, Plastic
- Dimensions (mm): 155x45x15
- Applications: Stripping
- Schmidt Pengukur Tegangan Digital (Alat Ukur Gaya Digital)Deskripsi:Electronic tension meter for hard to reach and limited access space applications. Available in two models: ETB (Basic unit) and ETX (with memory and outputs) Hand-held instrument with guide rollers up to max. 2000 m/min Tension meter with measuring head as small as possibleatribut:
- Measuring Principle: Strain gauge bridge
- Measuring Roller Deflection (mm): Max. 0.5
- Measuring Units: cN, g, N or lb, switchable
- Signal Processing: Digital
- KENTA Belt Tension Testeratribut:
- Tension Indicator: Colored LED Indication of High,Low and OK.
- Optional: RS-232C Data Cable with Software
- Accessories: Bletooth Data Adapter with Software
- Measurement (N): 0 to 750 (Newtons)
- Range: 0 to 120lb(Pounds)0 to 77kg(Kilograms)0 to 114Seems
- Belt Width (mm): Up to 36
- Accuracy: ±5% of full-scale
- Audible Warning: Piezoelectris Sounder
- Data Output: USB,RS-232,Bluetooth
- Dimensions (mm): 135x62x33
- Maximum Load: 850N
- Overload Alarm: 750N
- Power Supply: 4x1.5V AAA(UM-4)Battery
- Resolution: ±1(Least Significant Digit of Units)
- Standard: Main Unit
- BAHCO Tension Meter (Alat Ukur Presisi Gergaji)atribut:
- Thickness (mm): 35
- Total Length (mm): 170
- Width (mm): 110
- PLOT Belt Tension GaugeDeskripsi:A convenient gauge for adjusting the tension of Harley-Davidson drive belts.For harley* It is possible to measure the tension of the belt by using it to check the tension of the belt drive.atribut:
- Color: Anodized red
- YOKOGAWA Hybrid Electronic Meter (Panel Meter)atribut:
- Input (mA): 4–20
- Suffix: -32 Vle2
- TESTO Stainless Steel Pitot TubeDeskripsi:Product Includes: 1 x stainless steel Pitot tube, Ø 7 mm, length 1000 mm.atribut:
- Operating Temperature (°C): 0 to +600
- Product Color : Silver
- Product/Housing Material: Metal Housing
Daftar Harga belt tension meter Terbaru October 2026
| FACOM Belt Tension Meter | Rp8.399.900 |
| BANDO Belt Tension Meter (Alat Ukur Ketegangan Belt) | Rp3.499.900 |
| Gates Unitta Asia Sonic Belt Tension Meter | Rp19.999.900 |
| TESTO Moisture Meter (Alat Ukur Kelembaban) | Rp3.399.900 |
| OTC Belt Tension Gauge | Rp7.099.900 |
| AISIN Oil Pump | Rp879.900 |
| BANDO Belt Tension Meter Tension Master (Alat Ukur Ketegangan Belt) | Rp10.999.900 |
| RION Pocket Size Vibration Meter | Rp87.999.900 |
| Mitsuboshi Belting Non-contact sonic belt tension meter Doctor Tension Type-IV DRT-SH-F1 | Rp4.899.900 |
| Wipro Belt Tension Meter (Alat Ukur Ketegangan Belt) | Rp359.900 |
Data diperbarui pada 09/10/2026 (Harga belum termasuk PPN)




















































































































































/e8P102362512-3.jpg)

/6oP105736240-1.jpg)


/P102362220-1.jpg)


/nyP108520862-1.jpg)


/b4P109299400-1.jpg)

/67P102314223-2.jpg)

/rfP116006987-1.jpg)
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
/WD-40%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20333ml%201pc/60S000055216-2.jpg)
/OLFA%20Cutter%20Knife%20Safety%20(Pisau%20Cutter)%20149B%201pc/S009054721-2.jpg)
/Joyko%20Gel%20Ink%20Pen%20Q%20(Pulpen%20G2%20%2F%20Pulpen%20Gel)%20GP-265%20Black%200_5mm%201box(12pcs)/qmS009904958-2.jpg)
/REXCO%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20RX-SP0009%20500ml%2F415g%201pc/2bS000076083-4.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Sarung%20Tangan/Sarung%20Tangan%20Tahan%20Minyak/Sarung%20Tangan%20Tahan%20Minyak%20Karet%20Nitril/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)%2037-176%20Size%209%201pair/S000074366-1.jpg)

%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)/IKA%20(Copy%20Paper)%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20IKF%20PC%2070%20A4G%201ream/8pS035166313-2.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Kesehatan/Pertolongan%20Pertama%2C%20Kebutuhan%20Higienis/Perban%2C%20Kain%20Kasa/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)%201box(100pcs)/h6S039287618-2.jpg)
/3M%20Post-it%20654%20Sticky%20Notes%20(Kertas%20Memo)%20654-5CY%201pack(5pads)/5iS030245198-3.jpg)
/monotaro_id%20Lakban%20OPP%202inch%20(Solasi%20%2F%20Selotip)%20Transparent%2048mmx64m%201roll/h7S036166619-4.jpg)

/monotaro_id%20Cable%20Ties%204_8x250mm%20(Pengikat%20%2F%20Kabel%20Tis)%20White%201pack(100pcs)/2xS039549105-2.jpg)
/Max%20Stapler%20Needle%20(Isi%20Staples)%20No_10-1M%205%2F16x3%2F16Inch%201pack(20pcs)/S000005230-4.jpg)
/monotaro_id%20Plas%20Chamois%20(Lap%20Kanebo)%20with%20tube%20Yellow%2032x21cm%201pc/4uS037754174-2.jpg)